IFE/EIFE Interface Generic Commands
Get Current Time
The get current time command is not hardware protected. The get current time command is still enabled when the locking pad located on the front panel on the IFE/EIFE interface is in locked position.
To get the current time for all modules, set the command registers as follows:
|
Address |
Register |
Unit |
Type |
Range |
Description |
|---|---|---|---|---|---|
|
0x1F3F |
8000 |
– |
INT16U |
768 |
Command code = 768 |
|
0x1F40 |
8001 |
– |
INT16U |
10 |
Number of parameters (bytes) = 10 |
|
0x1F41 |
8002 |
– |
INT16U |
8704 |
Destination = 8704 (0x2200) |
|
0x1F42 |
8003 |
– |
INT16U |
0 |
Security type of the command |
|
0x1F43–0x1F44 |
8004–8005 |
– |
OCTET STRING |
0 |
Password of the command = 0 (no password required) |
The following registers contain the time data:
-
Register 8023 holds the month in the MSB, the day in the LSB.
-
Register 8024 holds the year offset in the MSB (add 2000 to get the year) and the hour in the LSB.
-
Register 8025 holds the minutes in the MSB, the seconds in the LSB.
-
Register 8026 holds the milliseconds.
Set Absolute Time
The set absolute time command is still enabled when the locking pad located on the front panel on the IFE/EIFE interface is in locked position.
To set the absolute time for all the IMU modules, set the command registers as follows:
|
Address |
Register |
Unit |
Type |
Range |
Description |
|---|---|---|---|---|---|
|
0x1F3F |
8000 |
– |
INT16U |
769 |
Command code = 769 |
|
0x1F40 |
8001 |
– |
INT16U |
18 |
Number of parameters (bytes) = 18 |
|
0x1F41 |
8002 |
– |
INT16U |
8704 |
Destination = 8704 (0x2200) |
|
0x1F42 |
8003 |
– |
INT16U |
0 |
Security type of the command |
|
0x1F43–0x1F44 |
8004–8005 |
– |
OCTET STRING |
0 |
Password of the command = 0 (no password required) |
|
0x1F45-0x1F48 |
8006–8009 |
– |
XDATE |
– |
Current date/time |
Write User Application Name
The user application name can be read from registers 10242 to 10273IMU Identification.
To write the user application name, set the command registers as follows:
|
Address |
Register |
Unit |
Type |
Range |
Description |
|---|---|---|---|---|---|
|
0x1F3F |
8000 |
– |
INT16U |
1032 |
Command code = 1032 |
|
0x1F40 |
8001 |
– |
INT16U |
– |
Number of parameters (bytes) = depends on the length of the user application name (up to 46 characters) |
|
0x1F41 |
8002 |
– |
INT16U |
0 |
Destination = 0 (0x0000) |
|
0x1F42 |
8003 |
– |
INT16U |
0 |
Security type of the command |
|
0x1F43–0x1F44 |
8004–8005 |
– |
OCTET STRING |
0 |
Password of the command = 0 (no password required) |
|
0x1F45–0x1F46 |
8006–8007 |
– |
INT32U |
– |
17039366 = User application name (load 0x0104 into register 8006, 0x0081 into 8007) |
|
0x1F46 |
8008 |
– |
INT16U |
2048 |
2048 |
|
0x1F48 |
8009 |
– |
OCTET STRING |
– |
|
|
0x1F49–0x1F5F |
8010–8038 |
– |
OCTET STRING |
– |
Depends on the length of the user application name and ends with the NULL character 0x00 |
Set Validity Duration of Data
This command is used to set the validity duration of data in the standard and legacy datasets.
The validity duration of data can be read in a register Validity Duration of Data.
To set the validity duration of data, set the command registers as follows:
|
Address |
Register |
Unit |
Type |
Range |
Description |
|---|---|---|---|---|---|
|
0x1F3F |
8000 |
– |
INT16U |
41868 |
Command code = 41868 |
|
0x1F40 |
8001 |
– |
INT16U |
12 |
Number of parameters (bytes) = 12 |
|
0x1F41 |
8002 |
– |
INT16U |
8705 |
Destination = 8705 (0x2201) |
|
0x1F42 |
8003 |
– |
INT16U |
1 |
Security type of the command |
|
0x1F43–0x1F44 |
8004–8005 |
– |
OCTET STRING |
– |
Password of the command: Administrator, Services, Engineer, or Operator user profile password |
|
0x1F45 |
8006 |
s |
INT16U |
5–300 (in steps of 5 s) |
Validity duration of data Factory setting: 10 s |