Maintenance Indicators
General Description
The BSCM module has 7 counters that help to manage the ComPacT NSX circuit breaker.
The BSCM module counters have the following properties:
-
All the counters are saved in non-volatile memory to prevent data loss in case of power loss.
-
The cumulating OF counter is read only. It stops incrementing when it reaches the maximum value 4 294 967 295.
-
The user can preset all counters (except the cumulating OF counter) to any value from 0 to 65535. The counters stop incrementing when they reach the maximum value 65535.
-
Tthe OF counter and close circuit breaker command counter have a threshold which can be set by the user, to any value from 0 to 65534.
The factory setting is 5000. An alarm is generated when a counter reaches the threshold.
BSCM Module Counters
|
Address |
Register |
RW |
X |
Unit |
Type |
Range |
Description |
|---|---|---|---|---|---|---|---|
|
0x023A– 0x023B |
571– 572 |
R |
1 |
– |
INT32U |
0–4 294 967 295 |
Cumulating OF counter (non-resettable open to close counter) |
|
0x023C |
573 |
R-WC |
1 |
– |
INT16U |
0–65535 |
OF counter (resettable open to close counter) |
|
0x023D |
574 |
R-WC |
1 |
– |
INT16U |
0–65535 |
SD counter (Close to SD position) |
|
0x023E |
575 |
R-WC |
1 |
– |
INT16U |
0–65535 |
SDE counter (Close to SDE position) |
|
0x023F |
576 |
R-WC |
1 |
– |
INT16U |
0–65535 |
Open circuit breaker command counter |
|
0x0240 |
577 |
R-WC |
1 |
– |
INT16U |
0–65535 |
Close circuit breaker command counter |
|
0x0241 |
578 |
R-WC |
1 |
– |
INT16U |
0–65535 |
Reset circuit breaker command counter |
|
0x0242–0x0243 |
579–580 |
– |
– |
– |
– |
– |
Reserved |
|
0x0244 |
581 |
R-WC |
1 |
– |
INT16U |
0–65535 |
OF counter threshold The factory setting is 5000. |
|
0x0245 |
582 |
R-WC |
1 |
– |
INT16U |
0–65535 |
Close circuit breaker command counter threshold The factory setting is 5000. |