Analog Inputs
Analog Input Register Mapping
The following table describes the analog inputs and corresponding registers and addresses of the IO module.
|
IO Module |
Analog Input Addresses |
Analog Input Registers |
|---|---|---|
|
IO 1 |
0x35FF–0x3668 |
13824–13929 |
|
IO 2 |
0x41B7–0x4220 |
16824–16929 |
Analog Input Registers of IO 1
The order and the description of the analog input registers of IO 2 are the same as those of IO 1.
|
Address |
Register |
RW |
Unit |
Type |
Range |
Description |
|---|---|---|---|---|---|---|
|
0x35FF–0x3600 |
13824–13825 |
– |
– |
– |
– |
Reserved |
|
0x3601–0x3602 |
13826–13827 |
R |
°C |
FLOAT32 |
-50–250 |
Analog input sensor Pt100 temperature value (updated once every 1 s) |
|
0x3603 |
13828 |
R |
– |
INT16U |
0–1 |
Data quality of the analog input
|
|
0x3604 |
13829 |
– |
– |
– |
– |
Reserved |
|
0x3605–0x3608 |
13830–13833 |
R |
– |
DATETIME |
– |
Timestamp of the last change of +/- 1 °C of the analog data value |
|
0x3609–0x360C |
13834–13837 |
– |
– |
– |
– |
Reserved |
|
0x360D–0x360E |
13838–13839 |
R |
°C |
FLOAT32 |
-50–250 |
Analog input Pt100 maximum value |
|
0x360F–0x3610 |
13840–13841 |
R |
°C |
FLOAT32 |
-50–250 |
Analog input Pt100 minimum value |
|
0x3611–0x3614 |
13842–13845 |
R |
– |
DATETIME |
– |
Timestamp of minimum value of analog input value recorded |
|
0x3615–0x3618 |
13846–13849 |
R |
– |
DATETIME |
– |
Timestamp of maximum value of analog input value recorded |
|
0x3619–0x361C |
13850–13853 |
R |
– |
DATETIME |
– |
Timestamp of last reset of min/max values of analog input value recorded |
|
0x361D–0x361E |
13854–13855 |
R |
– |
INT32U |
0–65534 |
Switchboard temperature threshold 1 counter This counter increments every time threshold 1 is exceeded. |
|
0x361F–0x3620 |
13856–13857 |
R |
– |
INT32U |
0–65534 |
Switchboard temperature threshold 2 counter This counter increments every time threshold 2 is exceeded. |
|
0x3621–0x3622 |
13858–13859 |
R |
– |
INT32U |
0–65534 |
Switchboard temperature threshold 3 counter This counter increments every time threshold 3 is exceeded. |
|
0x3623–0x363A |
13860–13883 |
R |
– |
OCTET STRING |
– |
Analog input identification coded over 45 ASCII characters(1) |
|
0x363B |
13884 |
R |
– |
INT16U |
0–2 |
Analog input type(1)
|
|
0x363C |
13885 |
– |
– |
– |
– |
Reserved |
|
0x363D–0x363E |
13886–13887 |
R |
°C |
FLOAT32 |
-50–250 |
Switchboard temperature threshold 1 pick-up value (Pt100) (1) Factory setting = 50 °C |
|
0x363F–0x3640 |
13888–13889 |
R |
s |
FLOAT32 |
1–3600 |
Switchboard temperature threshold 1 pick-up time delay (Pt100)(1) Factory setting = 10 s |
|
0x3641–0x3642 |
13890–13891 |
R |
°C |
FLOAT32 |
-50–250 |
Switchboard temperature threshold 1 drop-out value (Pt100)(1) Factory setting = 45 °C |
|
0x3643–0x3644 |
13892–13893 |
R |
s |
FLOAT32 |
1–3600 |
Switchboard temperature threshold 1 drop-out time delay (Pt100)(1) Factory setting = 10 s |
|
0x3645–0x3646 |
13894–13895 |
R |
°C |
FLOAT32 |
-50–250 |
Switchboard temperature threshold 2 pick-up value (Pt100)(1) Factory setting = 60 °C |
|
0x3647–0x3648 |
13896–13897 |
R |
s |
FLOAT32 |
1–3600 |
Switchboard temperature threshold 2 pick-up time delay (Pt100)(1) Factory setting = 10 s |
|
0x3649–0x364A |
13898–13899 |
R |
°C |
FLOAT32 |
-50–250 |
Switchboard temperature threshold 2 drop-out value (Pt100)(1) Factory setting = 55 °C |
|
0x364B–0x364C |
13900–13901 |
R |
s |
FLOAT32 |
1–3600 |
Switchboard temperature threshold 2 drop-out time delay (Pt100)(1) Factory setting = 10 s |
|
0x364D–0x364E |
13902–13903 |
R |
°C |
FLOAT32 |
-50–250 |
Switchboard temperature threshold 3 pick-up value (Pt100)(1) Factory setting = 70 °C |
|
0x364F–0x3650 |
13904–13905 |
R |
s |
FLOAT32 |
1–3600 |
Switchboard temperature threshold 3 pick-up time delay (Pt100)(1) Factory setting = 10 s |
|
0x3651–0x3652 |
13906–13907 |
R |
°C |
FLOAT32 |
-50–250 |
Switchboard temperature threshold 3 drop-out value (Pt100)(1) Factory setting = 65 °C |
|
0x3653–0x3654 |
13908–13909 |
R |
s |
FLOAT32 |
1–3600 |
Switchboard temperature threshold 3 drop-out time delay (Pt100)(1) Factory setting = 10 s |
|
0x3655–0x3656 |
13910–13911 |
R |
Ω |
FLOAT32 |
200–650 |
Motor temperature sensor fault threshold |
|
0x3657–0x3668 |
13912–13929 |
– |
– |
– |
– |
Reserved |
|
(1) Value set using EcoStruxure Power Commission software. |
||||||