Generic Commands
Change Output State
The command is used to change the state of IO module digital outputs assigned as user-defined outputs using EcoStruxure Power Commission software.
To change the output state, set the command registers as follows:
|
Address |
Register |
Unit |
Type |
Range |
Description |
|---|---|---|---|---|---|
|
0x1F3F |
8000 |
– |
INT16U |
1672 |
Command code = 1672 |
|
0x1F40 |
8001 |
– |
INT16U |
13 |
Number of parameters (bytes) = 13 |
|
0x1F41 |
8002 |
– |
INT16U |
– |
Destination =
|
|
0x1F42 |
8003 |
– |
INT16U |
1 |
Security type of the command |
|
0x1F43– 0x1F44 |
8004– 8005 |
– |
OCTET STRING |
– |
Password of the command: Administrator or Operator user profile password |
|
0x1F45 |
8006 |
– |
INT16U |
1–3 |
Output number
|
|
0x1F46 |
8007 |
– |
INT16U |
– |
Value to set:
|
Reset IO Module Alarm
The alarms can be read from the alarm status register.
To reset IO module alarms, set the command registers as follows:
|
Address |
Register |
Unit |
Type |
Range |
Description |
|---|---|---|---|---|---|
|
0x1F3F |
8000 |
– |
INT16U |
41099 |
Command code = 41099 |
|
0x1F40 |
8001 |
– |
INT16U |
10 |
Number of parameters (bytes) = 10 |
|
0x1F41 |
8002 |
– |
INT16U |
– |
Destination =
|
|
0x1F42 |
8003 |
– |
INT16U |
1 |
Security type of the command |
|
0x1F43– 0x1F44 |
8004– 8005 |
– |
OCTET STRING |
– |
Password of the command: Administrator or Operator user profile password |
Enable/Disable Simple Commands
To enable or disable the simple commands, set the command registers as follows:
|
Address |
Register |
Unit |
Type |
Range |
Description |
|---|---|---|---|---|---|
|
0x1F3F |
8000 |
– |
INT16U |
41100 |
Command code = 41100 |
|
0x1F40 |
8001 |
– |
INT16U |
11 |
Number of parameters (bytes) = 11 |
|
0x1F41 |
8002 |
– |
INT16U |
– |
Destination =
|
|
0x1F42 |
8003 |
– |
INT16U |
1 |
Security type of the command |
|
0x1F43– 0x1F44 |
8004– 8005 |
– |
OCTET STRING |
– |
Password of the command: Administrator or Operator user profile password |
|
0x1F45 |
8006 |
– |
INT16U |
– |
MSB: Enable or disable:
LSB: 0 (not used) |
Acknowledge Latched Output
To acknowledge the latched output, set the command registers as follows:
|
Address |
Register |
Unit |
Type |
Range |
Description |
|---|---|---|---|---|---|
|
0x1F3F |
8000 |
– |
INT16U |
41102 |
Command code = 41102 |
|
0x1F40 |
8001 |
– |
INT16U |
11 |
Number of parameters (bytes) = 11 |
|
0x1F41 |
8002 |
– |
INT16U |
– |
Destination =
|
|
0x1F42 |
8003 |
– |
INT16U |
1 |
Security type of the command |
|
0x1F43– 0x1F44 |
8004– 8005 |
– |
OCTET STRING |
– |
Password of the command: Administrator or Operator user profile password |
|
0x1F45 |
8006 |
– |
INT16U |
– |
MSB:
LSB: 0 (not used) |
Reset Analog Input Minimum/Maximum Values
The analog input maximum and minimum values can be read from the analog input registers.
To reset the minimum/maximum analog input values, set the command registers as follows:
|
Address |
Register |
Unit |
Type |
Range |
Description |
|---|---|---|---|---|---|
|
0x1F3F |
8000 |
– |
INT16U |
42890 |
Command code = 42890 |
|
0x1F40 |
8001 |
– |
INT16U |
10 |
Number of parameters (bytes) = 10 |
|
0x1F41 |
8002 |
– |
INT16U |
– |
Destination =
|
|
0x1F42 |
8003 |
– |
INT16U |
1 |
Security type of the command |
|
0x1F43– 0x1F44 |
8004– 8005 |
– |
OCTET STRING |
– |
Password of the command: Administrator or Operator user profile password |