Circuit Breaker Control Commands
Open Circuit Breaker
To open the circuit breaker with the communicating motor mechanism, set the command registers as follows:
|
Address |
Register |
X |
Unit |
Type |
Range |
Description |
|---|---|---|---|---|---|---|
|
0x1F3F |
8000 |
– |
– |
INT16U |
904 |
Command code = 904 |
|
0x1F40 |
8001 |
– |
– |
INT16U |
10 |
Number of parameters (bytes) = 10 |
|
0x1F41 |
8002 |
– |
– |
INT16U |
4353 |
Destination = 4353 (0x1101) |
|
0x1F42 |
8003 |
– |
– |
INT16U |
1 |
Security type of the command |
|
0x1F43–0x1F44 |
8004–8005 |
– |
– |
OCTET STRING |
– |
Password of the command: Administrator or Operator user profile password |
Close Circuit Breaker
To close the circuit breaker with the communicating motor mechanism, set the command registers as follows:
|
Address |
Register |
X |
Unit |
Type |
Range |
Description |
|---|---|---|---|---|---|---|
|
0x1F3F |
8000 |
– |
– |
INT16U |
905 |
Command code = 905 |
|
0x1F40 |
8001 |
– |
– |
INT16U |
10 |
Number of parameters (bytes) = 10 |
|
0x1F41 |
8002 |
– |
– |
INT16U |
4353 |
Destination = 4353 (0x1101) |
|
0x1F42 |
8003 |
– |
– |
INT16U |
1 |
Security type of the command |
|
0x1F43–0x1F44 |
8004–8005 |
– |
– |
OCTET STRING |
– |
Password of the command: Administrator or Operator user profile password |
Reset Circuit Breaker
To reset the circuit breaker with the communicating motor mechanism, set the command registers as follows:
|
Address |
Register |
X |
Unit |
Type |
Range |
Description |
|---|---|---|---|---|---|---|
|
0x1F3F |
8000 |
– |
– |
INT16U |
906 |
Command code = 906 |
|
0x1F40 |
8001 |
– |
– |
INT16U |
10 |
Number of parameters (bytes) = 10 |
|
0x1F41 |
8002 |
– |
– |
INT16U |
4353 |
Destination = 4353 (0x1101) |
|
0x1F42 |
8003 |
– |
– |
INT16U |
1 |
Security type of the command |
|
0x1F43–0x1F44 |
8004–8005 |
– |
– |
OCTET STRING |
– |
Password of the command: Administrator or Operator user profile password |
Enable/Inhibit a Circuit Breaker Close Order
To enable or inhibit a close order of the circuit breaker with the communicating motor mechanism, set the command register as follows:
|
Address |
Register |
X |
Unit |
Type |
Range |
Description |
|---|---|---|---|---|---|---|
|
0x1F3F |
8000 |
– |
– |
INT16U |
910 |
Command code = 910 |
|
0x1F40 |
8001 |
– |
– |
INT16U |
13 |
Number of parameters (bytes) = 13 |
|
0x1F41 |
8002 |
– |
– |
INT16U |
4353 |
Destination = 4353 (0x1101) |
|
0x1F42 |
8003 |
– |
– |
INT16U |
1 |
Security type of the command |
|
0x1F43–0x1F44 |
8004–8005 |
– |
– |
OCTET STRING |
– |
Password of the command: Administrator or Operator user profile password |
|
0x1F45 |
8006 |
– |
– |
INT16U |
1 |
|
|
0x1F46 |
8007 |
– |
– |
INT16U |
– |
Origin of the command: 256 = command sent via communication interface (IFM or IFE) |
Enable/Disable Automatic Reset
The user can read the automatic reset parameters at register 564 (bit 3).
To enable/disable automatic reset of the circuit breaker with the communicating motor mechanism, set the command registers as follows:
|
Address |
Register |
X |
Unit |
Type |
Range |
Description |
|---|---|---|---|---|---|---|
|
0x1F3F |
8000 |
– |
– |
INT16U |
42636 |
Command code = 42636 |
|
0x1F40 |
8001 |
– |
– |
INT16U |
12 |
Number of parameters (bytes) = 12 |
|
0x1F41 |
8002 |
– |
– |
INT16U |
4353 |
Destination = 4353 (0x1101) |
|
0x1F42 |
8003 |
– |
– |
INT16U |
1 |
Security type of the command |
|
0x1F43–0x1F44 |
8004–8005 |
– |
– |
OCTET STRING |
– |
Password of the command: Administrator user profile password |
|
0x1F45 |
8006 |
– |
– |
INT16U |
0–1 |
0 = automatic reset is not enabled. 1 = automatic reset is enabled. |
Enable/Disable Reset even if SDE
The user can read the reset parameters at register 564 (bit 4).
To enable/disable reset of the circuit breaker with the communicating motor mechanism even if SDE, set the command registers as follows:
|
Address |
Register |
X |
Unit |
Type |
Range |
Description |
|---|---|---|---|---|---|---|
|
0x1F3F |
8000 |
– |
– |
INT16U |
42637 |
Command code = 42637 |
|
0x1F40 |
8001 |
– |
– |
INT16U |
12 |
Number of parameters (bytes) = 12 |
|
0x1F41 |
8002 |
– |
– |
INT16U |
4353 |
Destination = 4353 (0x1101) |
|
0x1F42 |
8003 |
– |
– |
INT16U |
1 |
Security type of the command |
|
0x1F43–0x1F44 |
8004–8005 |
– |
– |
OCTET STRING |
– |
Password of the command: Administrator user profile password |
|
0x1F45 |
8006 |
– |
– |
INT16U |
0–1 |
0 = reset is not enabled if SDE = 1. 1 = reset is enabled even if SDE = 1. |