DOCA0213EN-02

Date Management

Introduction

Each module of the IMU uses its date to time-stamp events and history registers.

The date of the IMU modules is updated in two steps:

  1. External synchronization: The Modbus client synchronizes the IFM or IFE communication interface, or the BSCM Modbus SL/ULP module in Modbus SL only mode and in Modbus SL and ULP mode.

  2. Internal synchronization:

    • If the BSCM Modbus SL/ULP module is in ULP only mode, the IFM or IFE communication interface synchronizes all ULP modules connected in the IMU, including the BSCM Modbus SL/ULP module.

    • If the BSCM Modbus SL/ULP module is in Modbus SL only mode or in Modbus SL and ULP mode, the BSCM Modbus SL/ULP module synchronizes all ULP modules connected in the IMU.

External Synchronization

There are three ways to externally synchronize the IFM or IFE communication interface or the BSCM Modbus SL/ULP module in Modbus SL only mode or in Modbus SL and ULP mode:

  • Manually with EcoStruxure Power Commission software.

  • By programming of the Modbus client using:

    • either the Modbus function set date and time: function code 43-16 Write Functions

    • or the set absolute time command through the IFM or IFE communication interface, or through the BSCM Modbus SL/ULP module.

  • Automatically:

    • With IFE communication interface configured as SNTP mode.

The communication interface is considered as externally synchronized if the last synchronization has occurred within the last 2 hours.

NOTE: It is recommended to update the date and time of serial devices such as the IFM communication interface or the BSCM Modbus SL/ULP module periodically, by using the IFE communication interface webpages.

Internal Synchronization

The date and time is received from:

  • The IFM communication interface

  • Or the IFE communication interface

  • Or the BSCM Modbus SL/ULP module, in Modbus SL only mode or Modbus SL and ULP mode

The date and time is broadcast to all the ULP modules connected in the IMU.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?