List of BSCM Modbus SL/ULP Module Commands and Error Codes
List of Commands
The following table lists the available BSCM Modbus SL/ULP module commands, their corresponding command codes and user profiles. Follow the command execution procedures.
|
Command |
Command code |
User profile |
|---|---|---|
|
904 |
Administrator or Operator |
|
|
905 |
Administrator or Operator |
|
|
906 |
Administrator or Operator |
|
|
910 |
Administrator or Operator |
|
|
42636 |
Administrator |
|
|
42637 |
Administrator |
|
|
42638 |
Administrator |
|
|
42639 |
Administrator |
|
|
768 |
No password required |
|
|
769 |
No password required |
|
|
1024 |
No password required |
|
|
1032 |
Administrator |
|
|
41868 |
Administrator, Services, Engineer, or Operator |
Error Codes
Error codes generated by the BSCM Modbus SL/ULP module commands are returned in register 8021. In addition to generic error codes, the BSCM Modbus SL/ULP module commands generate the following error codes:
|
Error Code |
Description |
|---|---|
|
4363 (0x110B) |
BSCM Modbus SL/ULP module is out of order. |
|
4503 (0x1197) |
Circuit breaker is tripped. It must be reset before the command. |
|
4504 (0x1198) |
Circuit breaker is already closed. |
|
4505 (0x1199) |
Circuit breaker is already open. |
|
4506 (0x119A) |
Circuit breaker is already reset. |
|
4507 (0x119B) |
Actuator is in manual mode. Remote commands are not allowed. |
|
4508 (0x119C) |
Actuator is not present. |
|
4510 (0x119E) |
A previous command is still in progress. |
|
4511 (0x119F) |
Reset command is forbidden when SDE is set. |
|
4512 (0x11A0) |
Inhibit close order is enabled. |
Any other positive error code indicates an internal error.