BSCM Modbus SL/ULP Module Identification
Product Identification
|
Address |
Register |
RW |
X |
Unit |
Type |
Range |
Description |
|---|---|---|---|---|---|---|---|
|
0x4CD1 |
19666 |
R |
– |
– |
INT16U |
15149 |
Product identification = 15149 for the BSCM Modbus SL/ULP module |
BSCM Modbus SL/ULP Module Identifier
The BSCM Modbus SL/ULP module serial number is composed of a maximum of 15 alphanumeric characters with the following format: PPYYWWDLLLNNNNN.
-
PP = plant code
-
YY = year of fabrication (05–99)
-
WW = week of fabrication (01–53)
-
D = day of fabrication (1–7)
-
LLL = unique final assembly manufacturing line number or machine number within the plant (A–Z or 0–9).
-
NNNNN= unique product number generated on the day of manufacture by the plant manufacturing line or the plant machine (00001–99999).
A read request of eight registers is necessary to read the BSCM Modbus SL/ULP module serial number.
|
Address |
Register |
RW |
X |
Unit |
Type |
Range |
Description |
|---|---|---|---|---|---|---|---|
|
0x4CC8 |
19657 |
R |
– |
– |
OCTET STRING |
– |
‘PP’ |
|
0x4CC9 |
19658 |
R |
– |
– |
OCTET STRING |
05–99 |
‘YY’ |
|
0x4CCA |
19659 |
R |
– |
– |
OCTET STRING |
01–53 |
‘WW’ |
|
0x4CCB |
19660 |
R |
– |
– |
OCTET STRING |
1–7 |
‘D’ |
|
0x4CCC |
19661 |
R |
– |
– |
OCTET STRING |
A–Z, 0–9 |
‘LLL’ |
|
0x4CCD |
19662 |
R |
– |
– |
OCTET STRING |
00–99 |
‘NN’ |
|
0x4CCE |
19663 |
R |
– |
– |
OCTET STRING |
01–99 |
‘NN’ |
|
0x4CCF |
19664 |
R |
– |
– |
OCTET STRING |
01–99 |
‘N’ (the NULL character ends the serial number) |
BSCM Modbus SL/ULP Module Identification (Both Modbus and ULP Architecture)
The following table is valid for the three modes of the BSCM Modbus SL/ULP module:
-
Modbus SL only mode
-
ULP only mode
-
Modbus SL and ULP mode
|
Address |
Register |
RW |
Unit |
Type |
Range |
Description |
|---|---|---|---|---|---|---|
|
0x4C2B–0x4C34 |
19500–19509 |
R-WC |
– |
OCTET STRING |
– |
User application name = ComPacT NSX (by default) |
|
0x4C35–0x4C4A |
19510–19531 |
– |
– |
– |
– |
Reserved |
|
0x4C4B–0x4C8A |
19532–19595 |
R |
– |
OCTET STRING |
– |
Vendor URL = https://www.se.com/ |
|
0x4C8B–0x4C9A |
19596–19611 |
R |
– |
OCTET STRING |
– |
Product family = Gateway and server |
|
0x4C9B–0x4CA2 |
19612–19619 |
R |
– |
OCTET STRING |
– |
Product range = ComPacT NSX |
|
0x4CA3–0x4CAA |
19620–19627 |
R |
– |
OCTET STRING |
– |
Product model = BSCM Modbus SL/ULP |
|
0x4CAB–0x4CB2 |
19628–19635 |
R |
– |
OCTET STRING |
– |
Firmware revision |
|
0x4CB3–0x4CBC |
19636–19645 |
R |
– |
OCTET STRING |
– |
Vendor name = Schneider Electric |
|
0x4CBD–0x4CC6 |
19646–19655 |
R |
– |
OCTET STRING |
– |
Product code = LV434220 |
|
0x4CC7–0x4CD0 |
19656–19665 |
R |
– |
OCTET STRING |
– |
Serial number |
|
0x4CD1 |
19666 |
R |
– |
INT16U |
– |
Product identifier = 15149 for BSCM Modbus SL/ULP |
|
0x4CD2–0x4CDB |
19667–19676 |
R |
– |
OCTET STRING |
– |
Hardware revision |
|
0x4CDC–0x4CE5 |
19677–19686 |
R-WC |
– |
OCTET STRING |
– |
Product capability = Other (by default) |
|
0x4CE6–0x4CF5 |
19687–19702 |
R-WC |
– |
OCTET STRING |
– |
Product user tag = My tags (by default) |
BSCM Modbus SL/ULP Module Identification (Only Modbus Architecture)
The following table is valid for the two following modes:
-
Modbus SL only mode.
-
Modbus SL and ULP mode
|
Address |
Register |
RW |
Unit |
Type |
Range |
Description |
|---|---|---|---|---|---|---|
|
0x2800–0x2809 |
10241–10250 |
R-WC |
– |
OCTET STRING |
– |
User application name = ComPacT NSX (by default) |
|
0x280A–0x281F |
10251–10272 |
– |
– |
– |
– |
Reserved |
|
0x2D9D–0x2DDC |
11678–11741 |
R |
– |
OCTET STRING |
– |
Vendor URL = https://www.se.com/ |
|
0x2DDE–0x2DED |
11743–11758 |
R |
– |
OCTET STRING |
– |
Product family = Gateway and server |
|
0x2DEE–0x2DF5 |
11759–11766 |
R |
– |
OCTET STRING |
– |
Product range = ComPacT NSX |
|
0x2DF6–0x2DFD |
11767–11774 |
R |
– |
OCTET STRING |
– |
Product model = BSCM Modbus SL/ULP |
|
0x2DFE–0x2E05 |
11775–11782 |
R |
– |
OCTET STRING |
– |
Firmware revision |
|
0x2E2E–0x2E37 |
11823–11832 |
R |
– |
OCTET STRING |
– |
Vendor name = Schneider Electric |
|
0x2E38–0x2E41 |
11833–11842 |
R |
– |
OCTET STRING |
– |
Product code = LV434220 |
|
0x2E5B–0x2E64 |
11868–11877 |
R |
– |
OCTET STRING |
– |
Serial number |
|
0x2E7B |
11900 |
R |
– |
INT16U |
– |
Product identifier = 15149 for BSCM Modbus SL/ULP |
|
0x2E90–0x2E99 |
11921–11930 |
R |
– |
OCTET STRING |
– |
Hardware revision |
Read Device Identification
The Read Device Identification function is used to access in a standardized manner the information required to identify a device. The description is made up of a set of objects (ASCII character strings).
A complete description of the Read Device Identification function is available at www.modbus.org.
The coding for the identification of the BSCM Modbus SL/ULP module is the following:
|
Name |
Type |
Description |
|---|---|---|
|
Vendor name |
OCTET STRING |
‘Schneider Electric’ (18 characters) |
|
Product code |
OCTET STRING |
LV434220 |
|
Firmware revision |
OCTET STRING |
‘XXX.YYY.ZZZ’ |
|
Vendor URL |
OCTET STRING |
‘www.se.com’ |
|
Product name |
OCTET STRING |
BSCM Modbus SL/ULP (LV434220) |
|
Model name |
OCTET STRING |
Communication module |
|
User application name |
OCTET STRING |
ComPacT NSX (by default) |