DOCA0106EN-15

Set Device Time

Description

The Set Device Time page allows you to synchronize the date and time of the MasterPacT MTZ drawout circuit breaker connected to the EIFE interface to EIFE interface date and time. The time is set automatically. This page is used to get the MasterPacT MTZ drawout circuit breaker time.

List of Parameters in Set Device Time

Parameter

Description

Device Selection

Allows you to select the MasterPacT MTZ drawout circuit breaker that is to be synchronized with EIFE interface date and time.

Localized Time

Displays the time of the MasterPacT MTZ drawout circuit breaker.

Status

Displays the status of the MasterPacT MTZ drawout circuit breaker.

Get Time

Allows you to get time of the MasterPacT MTZ drawout circuit breaker.

Set Device Time

Not applicable.

Setting the Device Time

Step

Action

Table

1

From the EIFE webpage menu bar, click Control.

Opens the Control menu.

2

From the Control menu, click Set Device Time.

Opens the Set Device Time page.

3

Select the circuit breaker from the Set Device Time page and then click Get Time.

The date and time of the MasterPacT MTZ drawout circuit breaker gets synchronized with the EIFE interface date and time, and the status is updated as successful.

NOTE: If the synchronization fails, then the status is updated as unsuccessful.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.