IP Configuration
Description
The page allows you to set the IP parameters.
The users with Installer or Engineer roles can change the IP configuration settings.
Navigation to the IP Configuration Page
To view the page, click .
IPv4 Settings
|
Parameter |
Description |
|---|---|
|
|
Allows you to select the IPv4 configuration mode:
|
|
|
Allows you to select the mode for assigning the IPv4 parameters by using:
NOTE: While using a legacy DHCP server, the device name must be limited to 16 characters.
|
|
|
Used to enter manually the static IP address of an EIFE interface. |
|
|
Used to enter manually the Ethernet IP subnet mask address of your network. |
|
|
Used to enter manually the gateway (router) IP address used for wide area network (WAN) communication. |
IPv6 Settings
For IPv6 Configuration settings, after clicking , a pop-up message is displayed for confirmation to restart the interface to apply the new settings:
-
Click to restart and apply the setting changes.
-
Click to cancel the setting modifications and return to the last saved settings.
|
Parameter |
Description |
|---|---|
|
|
Enables IPv6 (Default setting: Enable). |
|
|
Static IP address of EIFE interface. NOTE: In the URL address box, use [ ] brackets to enter the link local address.
|
DNS Settings
|
Parameter |
Description |
|---|---|
|
|
Allows you to select the IPv4 configuration mode:
NOTE: Domain name system (DNS) is the naming system
for computers and devices connected to a local area network (LAN)
or the Internet.
|
|
|
Used to enter manually the IPv4 address of the primary DNS server. |
|
|
Used to enter manually the IPv4 address of the secondary DNS server. Used to perform a DNS resolution when the resolution fails with the primary DNS server. |