DOCA0106EN-16

User Interface Layout

Overview

This graphic shows the EIFE webpage user interface layout.

A

Header

B

Menu bar

C

Submenu bar

D

Webpages

E

Display zone

F

Action button

Header

The header displays the following information at the top of all the pages.

A

EIFE interface name

B

Intrusive command mode

C

Date and time

D

IP address

E

Device Location

F

My Profile

Logout

G

User name

Header Part

Description

EIFE interface name

Device name of the EIFE interface.

Intrusive command mode Intrusive Command Mode

  • : The intrusive command mode is Locked, the remote control commands are disabled.

  • : The intrusive command mode is Unlocked (default setting), the remote control commands are enabled.

Date and time

Current date in yyyy-mm-dd format.

Current time in hh-mm-sec format.

IP address

IPv4 address of the interface.

Device Location

Click Device Location to locate the selected interface in your equipment:

  • The ULP LED of the selected interface blinks for 15 seconds (test mode).

  • The icon blinks 1 second ON and 1 second OFF when the device location is activated.

My Profile

Click to change your account password in the Accounts Details Modification window.

Logout

Click to log out from the EIFE webpage session, or close your browser.

It is recommended to log out from the EIFE webpage session when it is not in use.

User name

Name of the user who has logged in.

Menu Bar

The main tabs in the menu bar are:

  • MONITORING & CONTROL

  • DIAGNOSTICS

  • SETTINGS

  • SECURITY

Submenu Bar

The subtabs in the submenu bar display the submenus under the selected main tab.

Webpages

The navigation menu under each subtab lists the webpages for the selected submenu.

Action Buttons

The action buttons correspond to the selected tab and it varies.

The following table describes the generic action buttons on Setting and Security webpages:

Button

Action

Apply Changes

Applies the setting changes.

Cancel Changes

Cancels the setting modifications and returns to the last saved settings.

For some settings, after clicking Apply Changes, a pop-up message is displayed for confirmation to restart the EIFE interface to apply the new settings:

  • Click Yes to restart and apply the setting changes.

  • Click No to cancel the setting modifications and return to the last saved settings.

Display Zone

The display zone shows the selected subtab in detail with all the related fields.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.