DOCA0106EN-15

Preferences

General Settings

Parameter

Description

Setting

Equipment Name

Displays the equipment name. This name is used in the web interface banner.

NOTE: The device name can be updated in the Name field of the Device Configuration submenu in the Configuration & Settings menu.

Real Time Sample Rate

Controls how often data is read from the device in the standard monitoring table views.

5...60 s

Default setting: 5 s

Communications Check Rate

Controls how often a communications check is performed while the browser is displaying real-time readings in the standard monitoring table views. This function attempts to bring any out-of-service devices back into service automatically.

5...30 min

Default setting: 15 min

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.