DOCA0106EN-16

Devices

Description

The DEVICES page gives the information about the MicroLogic control unit connected to the ULP port of the EIFE interface.

NOTE: The users with installer or engineer roles can change the Diagnostics page settings.

Navigation to the Devices Page

To view the DEVICES page, click DIAGNOSTICS > DEVICES

Circuit Breakers Parameters

Parameter

Description

Rated Current

Displays the rated current of the circuit breaker.

Protection Type

Displays the protection type of the circuit breaker.

Number of IO Module

Displays the number of IO modules connected to the circuit breaker.

Remaining service life indicator

Displays the remaining service life of circuit breaker.

Contact wear indicators

Displays the contact wear counters of the circuit breaker.

Indication contacts (OF) operation since last reset

Displays the indication of contact operation of circuit breaker since last reset.

Fault trip indication contact (SDE) operation

Displays the indication of fault trip contact operation of circuit breaker.

Cradle connected

Displays the status of cradle in connected position.

Cradle disconnected

Displays the status of cradle in disconnected position.

Cradle test

Displays the status of cradle in test position.

Components Parameters

Device

Parameter

Description

Circuit Breaker

Product Range

Name of the device type.

Product Model

Device model number.

Serial Number

Device serial number.

Commercial Reference Number

Device commercial reference number.

Firmware Revision

Current firmware version.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.