DOCA0106EN-16

Device Log Export

Description

The Device Log Export page is used to export the device logs automatically by EIFE interface. The device log export allows you to configure EIFE interface to export device logs periodically. You can choose to export the device log files through email or FTPS.

NOTE: If the email and the FTPS servers are not located on the same Ethernet network segment as the EIFE interface, ensure that the EIFE interface default gateway is properly configured.

Transport

Parameter

Description

Setting

Disabled

When Disabled is selected, either email or FTPS is enabled.

Email

Allows you to export the log files through email.

FTPS

Allows you to export the log files through FTPS.

Incremental

Selects only the new interval data logged since the last successful data export.

NOTE:
  • If the transport is scheduled for Hourly or Logging Interval, the incremental check box is selected automatically and is unavailable to be cleared.

  • If the Incremental check box is not selected, the complete log file is sent through an email as an attachment on each scheduled interval.

Manual Export

Allows you to export the accumulated log files manually.

Schedule

Parameter

Description

Setting

Logging Interval

Selects how often the data logs are sent.

  • Hourly

  • Daily

  • Weekly

  • Monthly

  • Logging Interval

To Addresses

Parameter

Description

Setting

To Addresses

Lists the email recipients configured in the EIFE interface user accounts.

FTPS Parameters

Parameter

Description

Setting

Server IP Addresses

Allows you to enter the FTPS server IP address.

Server TCP Port

Allows you to enter the server port number.

Directory

Allows you to select the directory where you want the files to be saved.

Username

Allows you to enter the FTPS username.

Password

Allows you to enter the FTPS password.

Passive

Allows you to select the mode of FTPS operation.

NOTE: Passive mode is enabled by default.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.