DOCA0106EN-16

Firmware Update

Read the following instructions carefully before performing the firmware update to version 005:

  • Firmware update to version 005 is recommended when all the features available in firmware version 004 are also available in firmware version 005.

  • Firmware update to version 005 is not recommended when any of the features currently used by the application in firmware version 003 is not available in firmware version 005.

NOTE: To use EIFE interface with MicroLogic Active control unit, you must update the EIFE interface firmware to version 005.003.000 or later.

Description

Use the latest version of EcoStruxure Power Commission software for all firmware updates.

The latest version of EIFE interface firmware and EIFE webpages are updated in a single operation through EcoStruxure Power Commission software.

For more information on EIFE interface firmware versions, refer to the DOCA0147EN Enerlin'X IFE/EIFE - Ethernet Interface - Firmware Release Notes.

NOTICE
LOSS OF DATA
  • Ensure that you take backup of the data log files before updating the firmware. The data log entries of the EIFE interface may be lost when the EIFE interface firmware is updated.
  • Ensure that you take backup of data present in User Accounts and Email Events sections of EIFE webpages.
  • Ensure that after firmware upgrade, you restore the User Accounts and Email Events configuration on EIFE webpages.
Failure to follow these instructions can result in permanent loss of data.

After updating the firmware of one device in the IMU, use the latest version of EcoStruxure Power Commission software to check the firmware compatibility between the IMU devices. The Firmware Update table helps you to diagnose and identify all discrepancy issues between the IMU devices. This table also provides the recommended actions relevant to the detected discrepancies.

NOTE: After updating the firmware of EIFE interface from version 003 or 004 to 005, the user name and password of the EIFE interface changes to default. When you access EIFE interface for the first time after the firmware update, you are asked to change the default password. For more information, refer to First Access Through PC with Windows 10 and Later.

Signed Firmware

All firmware designed for the MasterPacT MTZ IMU is signed using the Schneider Electric public key infrastructure.

The digital certificates used to authenticate genuine Schneider Electric firmware and software must be regularly verified to ensure that they are still valid. Digital certificates that are no longer valid are published on the certificate revocation list (CRL) available on the Schneider Electric Cybersecurity Support Portal.

NOTE: Each time you connect to the MicroLogic X or MicroLogic Active control unit using EcoStruxure Power Commission software, the digital signature of the control unit is automatically verified.

For more information on cybersecurity for the MasterPacT MTZ circuit breakers, refer to the MasterPacT MTZ – Cybersecurity Guide in Related Documents.

Checking the Firmware Version

You can find the firmware version of the devices in the IMU using:

  • EcoStruxure Power Commission software, refer to the EcoStruxure Power Commission Online Help.

  • EIFE webpages, refer to the following procedure:

    1. Sign in to the EIFE webpage.

    2. Do one of the following:

      • Navigate to Diagnostics > Device Identification > Firmware version.

      • Navigate to Diagnostics > EIFE > Firmware Revision.

NOTE: If you have updated the firmware recently, press F5 to refresh the webpage and update the displayed firmware number.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.