DOCA0106EN-15

User Management

Description

The USER MANAGEMENT page is only accessible to the user with Security Administrator (SECADM) role.

The users with Security Administrator role can:

  • Create, edit, and delete user accounts.

  • Assign a role and a password to the users.

NOTE: User accounts can also be managed by using the EcoStruxure Cybersecurity Admin Expert Software.

Navigation to the User Management Page

To view the USER MANAGEMENT page, click SECURITY > USER MANAGEMENT.

Security Administrator Role

The Security Administrator user account is created by default with all the roles. Therefore, EIFE interface helps to ensure that at least one user with SECADM role is always present in the users list.

WARNING
POTENTIAL COMPROMISE OF SYSTEM AVAILABILITY, INTEGRITY, AND CONFIDENTIALITY
Change default passwords at first use to help prevent unauthorized access to device settings, controls, and information.
Failure to follow these instructions can result in death, serious injury, or equipment damage.

The Security Administrator default password is AAAAAAAA.

User Account Parameters

Parameter

Description

User Name

Enter a name for a new user.

  • User name is composed of 4 to 16 characters.

  • User names are case-sensitive and can contain special characters.

Password

Enter the password for the new user Password Syntax. The password entered must be confirmed.

Role

Select one or multiple roles for the new user in the predefined list of roles Role Based Access Control.

Email ID

Enter a valid email address for the entered user name.

User Account Edition

Once the user account is created, click the icon to edit and complete it with the following parameters.

Parameter

Description

User Name

Edit the user name.

Role

Change the role.

EmailID

Edit the email address of the user.

Phone

Enter the phone number of the user.

Language

Select the user language in the predefined list of languages.

Unlock

Unlock the user account locked after entry of 3 incorrect passwords.

Enabled

Turn on to enable the user account.

User Account Details

Once the user account is created, click the icon to view the following parameters.

Parameter

Description

User Name

Displays name of the user.

EmailID

Displays the email address of the user.

Language

Displays the selected language of the user.

Phone

Displays the phone number of the user.

UserStatus

Displays the user status.

PasswordExpiryTime

Displays the expiration time of user password.

LockedUntil

Displays the user account locked status.

Password Syntax

A password is composed of 8 to 16 characters. It is case-sensitive and the allowed characters are:

  • Digits from 0 to 9

  • Letters from a to z

  • Letters from A to Z

  • Special characters as *, /, \, and so on.

To be accepted by EIFE interface, a password must contain one letter lowercase, one letter uppercase, one digit and one non-alphanumeric character.

NOTE: Password with eleven stars (***********) is not allowed. While editing a user password, the three previous passwords of this user cannot be used.

Password Update

Once created by the user with Security Administrator role, the credentials are shared by Security Administrator with the new user.

WARNING
POTENTIAL COMPROMISE OF SYSTEM AVAILABILITY, INTEGRITY, AND CONFIDENTIALITY
Change default passwords at first use to help prevent unauthorized access to device settings, controls, and information.
Failure to follow these instructions can result in death, serious injury, or equipment damage.

The new user will be prompted to change his password at first connection. The password can be changed anytime by the user in the MyProfile window.

Password Reset

A user with Security Administrator role can reset another user password by pressing the Reset button in the webpage. The new password is generated automatically and is shown in a pop-up message. Once generated, the new password is shared by Security Administrator with the user. The user must customize his new password at the first connection.

For more information about resetting the Security Administrator password, refer to Reset Button.

In the case that all passwords with Security Administrator roles are lost or forgotten, contact your local Schneider Electric Customer Care Center.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?