DOCA0106EN-15

About the Document

Document Scope

The aim of this document is to provide the users, installers, and the maintenance personnel with the technical information and procedure needed to access and maintain the EIFE Embedded Ethernet interface for MasterPacT MTZ drawout circuit breakers.

Validity Note

This guide is valid for the EIFE interface for use with:

  • MasterPacT MTZ circuit breakers with MicroLogic X control unit

  • MasterPacT MTZ circuit breakers with MicroLogic Active control unit

Online Information

The information contained in this guide is likely to be updated at any time. Schneider Electric strongly recommends that you have the most recent and up-to-date version available on www.se.com/ww/en/download.

The technical characteristics of the devices described in this guide also appear online. To access the information online, go to the Schneider Electric Country website at www.se.com.

General Cybersecurity Information

In recent years, the growing number of networked machines and production plants has seen a corresponding increase in the potential for cyber threats, such as unauthorized access, data breaches, and operational disruptions. You must, therefore, consider all possible cybersecurity measures to help protect assets and systems against such threats.

To help keep your Schneider Electric products secure and protected, it is in your best interest to implement the cybersecurity best practices as described in the Cybersecurity Best Practices document.

Schneider Electric provides additional information and assistance:

Product Related Cybersecurity Information

WARNING
POTENTIAL COMPROMISE OF SYSTEM AVAILABILITY, INTEGRITY, AND CONFIDENTIALITY
  • Change default passwords at first use to help prevent unauthorized access to device settings, controls, and information.
  • Disable unused ports/services and default accounts to help minimize pathways for malicious attackers.
  • Place networked devices behind multiple layers of cyber defenses (such as firewalls, network segmentation, and network intrusion detection and protection).
  • Use cybersecurity best practices (for example, least privilege, separation of duties) to help prevent unauthorized exposure, loss, modification of data and logs, or interruption of services.
Failure to follow these instructions can result in death, serious injury, or equipment damage.

Environmental Data

For product compliance and environmental information, refer to the Schneider Electric Environmental Data Program.

Available Languages of the Document

The document is available in these languages:

Related Documents

Title of the Documentation

Reference Number

Enerlin'X EIFE – Embedded Ethernet Interface for One MasterPacT MTZ Drawout Circuit Breaker – Instruction Sheet

NVE23550

Enerlin'X IFE/EIFE - Ethernet Interface - Firmware Release Notes

DOCA0147EN

ULP (Universal Logic Plug) System - User Guide

MasterPacT, ComPacT, PowerPacT Circuit Breakers - Modbus Communication - User Guide

MasterPacT MTZ - MicroLogic X Control Unit - User Guide

MasterPacT MTZ - MicroLogic Active Control Unit - User Guide

Breaker Communication and Isolation Module (BCIM) for MicroLogic Active Control Unit - User Guide

MasterPacT MTZ Circuit Breakers with MicroLogic X Control Units - IEC 61850 Communication Guide

CET850 IEC 61850 Configuration Software – User Manual

SEPED306025EN

Enerlin'X IO - Input/Output Application Module for One Circuit Breaker - User Guide

MasterPacT, ComPacT, PowerPacT - Cybersecurity Guide

EcoStruxure Cybersecurity Admin Expert Guide

CAE_UM_EN

To find documents online, visit the Schneider Electric download center (www.se.com/ww/en/download/).

Information on Non-Inclusive or Insensitive Terminology

As a responsible, inclusive company, Schneider Electric is constantly updating its communications and products that contain non-inclusive or insensitive terminology. However, despite these efforts, our content may still contain terms that are deemed inappropriate by some customers.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.