DOCA0106EN-15

Indicators

Description

The Indicators page provides the maintenance counter information for the MasterPacT MTZ drawout circuit breaker connected to the EIFE interface. The page displays the information about the remaining service life of the circuit breaker, contact wear counters, circuit breaker operation counters, and the cradle counters.

Viewing Maintenance Counters

Step

Action

Result

1

From the EIFE webpage menu, click Maintenance.

Opens the Maintenance page.

2

From the Indicators menu, select the circuit breaker from the device list.

NOTE: This feature is available for circuit breakers only.

Displays the information about the remaining service life of the circuit breaker, contact wear counters, circuit breaker operation counters, and the cradle counters.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.