DOCA0106EN-15

Date and Time

Description

The Date and Time page allows you:

  • To manually set the date and time of the MasterPacT MTZ drawout circuit breaker connected to the EIFE interface

  • To automatically synchronize the date and time of the MasterPacT MTZ drawout circuit breaker to the EIFE interface time

  • To periodically check the synchronization at specified interval of time

List of Parameters in Date and Time Configuration

Parameter

Description

Manual

Allows you to select the manual date and time setting of the MasterPacT MTZ drawout circuit breaker. This option is disabled when Automatic is selected.

Date

Allows you to set the present date manually in the format yyyy-mm-dd.

Time

Allows you to set the present time manually in the format hh:mm:sec.

Automatic (SNTP)

Allows you to enable the automatic time setting of the MasterPacT MTZ drawout circuit breaker. This option is disabled when Manual is selected.

Poll Interval

Allows you to enter the poll interval in hours that ranges from 1 through 63.

Obtain Servers Automatically via DHCP/BOOTP

Allows you to enable the check box that obtains the server address from DHCP or BOOTP.

Primary SNTP/NTP server

Allows you to enter the primary SNTP server address.

Secondary SNTP/NTP server

Allows you to enter the secondary SNTP server address.

Apply

Allows you to automatically synchronize the time of the MasterPacT MTZ drawout circuit breaker connected to the EIFE interface with the EIFE interface time.

Cancel

Allows you to clear the synchronization of the MasterPacT MTZ drawout circuit breaker connected to the EIFE interface.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.