DOCA0106EN-16

Hardware Description

Description

A

Two RJ45 Ethernet ports

 

A1 OFF: 10 Mbps

Steady green: 100 Mbps

 

A2 Steady green: link

Blinking green: activity

B

Reset button

C

Device identification label

D

Module status LED

E

Network status LED

F

ULP status LED

G

USB mode ULP port

H

QR code to product information

I

DIN clip

J

Grounding connection

K

CT limit switch

L

CE limit switch

M

CD limit switch

N

MAC ID

For information on installation, refer to the instruction sheet – NVE23550.

Mounting

The EIFE interface is embedded in the cradle of the MasterPacT MTZ circuit breaker.

Power Supply

The EIFE interface is powered by the ULP port module.

For more information, refer to ULP System User Guides in Related Documents.

It is recommended to use an UL listed and recognized limited voltage/limited current or a class 2 power supply with a 24 Vdc, 3 A maximum.

NOTE: For 24 Vdc power supply connection, use copper conductors only.

Ethernet Connection

Module Status LED

The module status dual color LED, indicates the EIFE interface status.

LED Indication

Status Description

Action

OFF

No power

None

Steady green

EIFE interface operational

None

Blinking green (250 ms ON, 250 ms OFF)

Hidden control webpage available

None

Blinking green (500 ms ON, 500 ms OFF)

EIFE interface firmware corrupted

Contact your local Schneider Electric service team for support.

Blinking red (500 ms ON, 500 ms OFF)

EIFE interface in degraded mode

Replace ULP module at the next maintenance operation.

Steady red

EIFE interface out of service

None

Blinking green/red (1 s green, 1 s red)

Firmware update in progress

None

Blinking green/red (250 ms green, 250 ms red)

Self-test in progress

None

Network Status LED

The network status dual color LED, indicates the Ethernet network status.

LED Indication

Status Description

OFF

No power or no IP address

Steady green

Valid IP address

Steady red

Duplicated IP address

Blinking green/red (250 ms green, 250 ms red)

Self-test in progress

Steady amber

Error detected in IP configuration

ULP Status LED

The yellow ULP status LED describes the mode of the ULP module.

ULP LED

Mode

Action

Nominal

None

Conflict

Remove extra ULP module

Degraded

Replace EIFE interface at the next maintenance operation

Test

None

Non-critical firmware discrepancy

Use the EcoStruxure Power Commission software to check the firmware and hardware compatibility and follow the recommended actions.

Non-critical hardware discrepancy

Configuration discrepancy

Install missing features

Critical firmware discrepancy

Use the EcoStruxure Power Commission software to check the firmware and hardware compatibility and follow the recommended actions

Critical hardware discrepancy

Stop

Replace EIFE interface

Power OFF

Check power supply

Modbus Address

The EIFE interface accepts the Modbus address of the IMU to which it is connected. The Modbus address is 255 and cannot be changed.

Intrusive Command Mode

The EIFE interface intrusive command mode can be configured with EcoStruxure Power Commission software. This software can enable or disable the ability to send the remote control commands over the Ethernet network to the EIFE interface, and to the other modules of the connected IMU.

  • If the intrusive command mode is Locked, the remote control commands are disabled.

  • If the intrusive command mode is Unlocked (default setting), the remote control commands are enabled.

NOTE: Whatever is the intrusive command mode, the only remote control command that is always enabled is the Set Absolute Time command.

Reset Button

The Reset button has three functions, according to the duration of the button pressed.

Time Range

Function

1 s

Resets the IP acquisition mode to its default setting (DHCP).

5 s

Resets the security administrator password to its default setting (AAAAAAAA).

NOTE: If a security administrator role does not already exist, executing this action will create a new security administrator role.

10 s

Resets the EIFE interface to its factory default settings.

Security Administrator Password Reset

The following procedure describes the steps to reset the security administrator password to its default setting:

  1. Press the reset button (R) on the EIFE interface for 5 s. The LED light will flash rapidly in a pattern alternating between red and green, with each color displayed for 100 ms.

  2. On releasing the reset button (R), the EIFE interface will enter reset mode for a duration of 30 s and prompts the user to reset the password to its default setting. The LED light will flash rapidly in a pattern alternating between red and green, with each color displayed for 100 ms.

  3. Press the reset button (R) on the EIFE interface to confirm or wait for 30 s to cancel the reset.

  4. Once the reset of the security administrator password is confirmed, either the password is reset to the default setting (AAAAAAAA) or a new security administrator role is added.

NOTE:

Every time a reset operation is successfully performed, the reset administrator password counter increments by one.

EIFE Interface Factory Reset

The following procedure describes the steps to reset the EIFE interface to its factory default settings:

  1. Press the reset button (R) on the EIFE interface for 10 s. The LED will rapidly flash in red with a 100 millisecond ON and 100 ms OFF interval.

  2. On releasing the reset button (R), the EIFE interface will enter reset mode for a duration of 30 s and prompts the user to reset the device to its factory default settings. The LED will rapidly flash in red with a 100 ms ON and 100 ms OFF interval.

  3. Press the reset button (R) on the EIFE interface to confirm or wait for 30 s to cancel the reset.

  4. Once the reset to factory default settings is confirmed, the EIFE interface reboots and all the device settings are reset to their factory default values.

After reset, the EIFE interface restarts and restores the following settings to their factory default values:

Parameter

Default Value

Date & Time

  • Date and time setting mode: Manual

  • Date: yyyy-mm-dd

  • Time: hh:mm:sec

NTP

  • NTP server setting mode: Manual

  • Primary SNTP: time.windows.com

  • Secondary SNTP: time.nist.com

Time zone

  • Time zone offset :UTC

  • Day light saving: Disabled

Preferences

  • Real time sample rate : 5 s

  • Communications check rate: 15 min

Ethernet

Frame format: Auto

Port control

  • ETH1 mode: Auto-negotiation

  • ETH2 mode: Auto-negotiation

Broadcast storm protection

  • Enable: Enabled

  • Level: Medium-Low

  • Committed information rate: 4000 s

IP configuration

IPv4

  • Configuration: Automatic

  • Mode: DHCP

  • IP address: 169.254.xxx.yyy (xxx.yyy = last 6 bytes of MAC address)

  • Subnet mask: 255.255.0.0

  • Gateway: 0.0.0.0

IPv6

  • Enable IPv6: Enabled

  • IPv6 address: Unavailable

DNS

  • DNS address: Automatic

Email service

Email service: Disabled

Data publishing

Logging interval: Disabled

RSTP

RSTP: Disabled

SNMP

SNMPV1 agent: Disabled

Devices

  • Name: Last 6 digits of MAC ID

  • IP address: Default

  • Breaker unit name field is empty.

  • Data publishing: Disabled

Contact management

Empty user email list

IP network services

  • Modbus TCP: Enabled

  • Secure commissioning: Disabled

  • Secure Modbus for M2M: Disabled

  • FTPS server: Disabled

  • Discovery: Enabled

  • HTTP/Web: Disabled

  • HTTPS: Enabled

Modbus TCP/IP filtering

  • Modbus TCP/IP filtering: Disabled

  • IP filtering exception list cleared

Certificates

Certificate type: Self signed

User management

  • User name: SecurityAdmin

  • Roles: SECADM, Viewer, Operator, Engineer, Installer

  • Password: AAAAAAAA

Syslog service

Syslog logging service: Disabled

Cradle Position Contacts

To identify the cradle position of the circuit breaker, the EIFE interface has three limit switches.

Limit Switch

Description

CE

Cradle connected position contact

CD

Cradle disconnected position contact

CT

Cradle test position contact

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.