DOCA0106EN-16

Webpage Description

MONITORING & CONTROL Webpage

Submenu

Table updated@D1

Webpage

Description

CIRCUIT BREAKERS

  • Displays data from the circuit breaker.

  • Allows you to reset of minimum and maximum values.

  • Allows you to control the circuit breaker.

IO MODULES

-

  • Displays data from the IO modules.

  • Allows you to control the IO modules.

  • Displays Input/Output configuration for IO modules connected to the EIFE interface.

DIAGNOSTICS Webpage

Submenu

Webpage

Description

COMMUNICATION

STATUS

Displays diagnostic data used to troubleshoot the network-related problems.

ETHERNET

Displays the diagnostic data of Ethernet global statistics and Ethernet port characteristics.

MODBUS

Displays the global statistics of TCP/IP and TCP port connections.

ULP

Displays the global statistics of ULP port connection.

REDUNDANCY-RSTP BRIDGE

Displays the diagnostic data of RSTP bridge.

REDUNDANCY-RSTP PORTS

Displays the diagnostic data of RSTP ports.

SNMP

Displays the diagnostic data of SNMPV1 Agent.

Read Device Registers

Displays register data connected locally to the EIFE interface.

EIFE

  • Displays the EIFE interface basic information.

  • Displays the EIFE interface parameters and characteristics.

DEVICES

CIRCUIT BREAKERS

  • Displays the list of the IMU devices connected to the ULP port.

  • Displays the maintenance counter information of the selected device.

  • Displays the details of circuit breaker communication component.

SETTINGS Webpage

Submenu

Webpage

Description

GENERAL

COMMUNICATION

DATE & TIME

Sets the date and time manually or sets the EIFE interface time automatically using an NTP source or configures the device connected to EIFE interface to synchronize their time with the EIFE interface time automatically.

TIME ZONE

Sets the time zone for the region and sets the daylight saving time.

ETHERNET

Sets the Modbus TCP/IP communication interface.

IP CONFIGURATION

Sets the IP parameters.

EMAIL SERVICE

Sets the configuration of SMTP server for mailing purpose.

DATA PUBLISHING

Sets data generation and publishing parameters.

REDUNDANCY-RSTP

Sets the RSTP bridge and RSTP port details.

SNMP

Sets the SNMPV1 agent parameters.

DEVICES

-

  • Sets the EIFE interface name.

  • Sets circuit breaker name and data logging.

CONTACT MANAGEMENT

EMAILS

  • Sets the email address for the events notification and data publishing.

  • Sets the events to be notified.

SECURITY Webpage

Submenu

Webpage

Description

IP NETWORK SERVICES

-

Configures the settings and activates the IP network services.

MODBUS TCP/IP FILTERING

-

Configures the IP addresses that can access the EIFE interface through Modbus TCP/IP.

CERTIFICATES

-

Displays the EIFE interface certificate with expiration date and validity period.

USER MANAGEMENT

-

Manages the existing and newly added user accounts.

SYSLOG SERVICE

-

Configures the Syslog server address.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.