DOCA0106EN-15

Security Logs

Description

The security log feature of the EIFE interface enables the generation of security related events such as successful or failed login attempts, user configuration, object access, and firmware updates. These events are recorded in security logs which provide information that can be used to monitor activities carried out on the system. The security team can use this information to detect and respond in the event of a security compromise.

The security team can retrieve the generated security logs by:

  • Using the manual export option on the EIFE webpage. For more information, refer to Export to CSV.

  • Configuring the Syslog parameters in the EIFE webpage. In this case, the generated security logs will be automatically sent to the configured Syslog server. For more information, refer to Syslog Service Parameters.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.