DOCA0106EN-16

Webpage Description

Monitoring Webpage

Monitoring Submenu

Webpage

Description

Real Time Data

Single Device Pages

The single device pages provide basic readings of the MasterPacT MTZ drawout circuit breaker connected to the EIFE interface.

Summary Device Pages

The summary device pages provide summaries of the MasterPacT MTZ drawout circuit breaker connected to the EIFE interface.

Trending

The trending page view provides real-time graphic and table trending of the MasterPacT MTZ drawout circuit breaker connected to the EIFE interface.

Device Logging

Single Device Pages

The single device pages provide the graphic and table trending logs of user-selectable quantities for the MasterPacT MTZ drawout circuit breaker connected to the EIFE interface.

Summary Device Pages

The summary device pages provide graphic trending logs of MasterPacT MTZ drawout circuit breaker connected to the EIFE interface.

Control Webpage

Control Submenu

Webpage

Description

Device Control

Device Control

Resets and controls the MasterPacT MTZ drawout circuit breaker connected to the EIFE interface.

Set Device Time

Set Device Time

Displays the time of the MasterPacT MTZ drawout circuit breaker connected to the EIFE interface.

Diagnostics Webpage

Diagnostics Submenu

Webpage

Description

General

Statistics

Displays diagnostic data used to troubleshoot the network-related problems.

Product Information

Device Identification

  • Displays the EIFE interface basic information to set the EIFE interface device name and helps in the device physical location.

  • Contains information about the product name, serial number, model number, firmware version, unique identifier, MAC address, IPv4 address, and IPv6 link local address.

IMU Information

Displays the list of the IMU devices connected to the ULP port.

Device Health Check

Read Device Registers

Displays register data connected locally to the EIFE interface.

Communications Check

Verifies the communication health of the MasterPacT MTZ drawout circuit breaker connected to the EIFE interface.

IO Readings

IO Readings

Displays the status of IO module connected to the MasterPacT MTZ drawout circuit breaker. Displays No IO modules connected if the MasterPacT MTZ drawout circuit breaker is not connected to a IO module.

NOTE: IO Module refers to the MasterPacT MTZ drawout circuit breaker name defined in the Device List page.

Maintenance Webpage

Maintenance Submenu

Webpage

Description

Indicators

Indicators

Displays the maintenance counters of the MasterPacT MTZ drawout circuit breaker connected to the EIFE interface.

Configuration & Settings Webpage

Configuration & Settings Submenu

Webpage

Description

General

Device Physical Location

  • Locate the EIFE-XXYYZZ interface.

  • Click Blink ON.

  • The ULP LED of the EIFE-XXYYZZ interface blinks and is active for 15 s (Test mode: 1 s ON, 1 s OFF).

Date and Time

Sets the date and time manually or sets the EIFE interface time automatically using an SNTP source or configures the ULP devices connected to EIFE interface to synchronize their time with the EIFE interface time automatically.

Time Zone

Configures the time zone for the region and sets the daylight saving time.

Network Configuration

Ethernet Configuration (Dual port)

Configures the Ethernet.

IP Configuration

Configures the IP parameters.

Modbus TCP/IP Filtering

Configures the maximum number of Modbus TCP/IP server connections. Configures the IP addresses that can access the EIFE interface through Modbus TCP/IP.

Email Configuration

Email Server Configuration

Configures the alarms to be emailed.

Configures the SMTP parameter for mailing purpose.

Email Events

Configures the alarms to be sent through email.

Device Configuration

Device List

Configures MasterPacT MTZ drawout circuit breaker connected to the EIFE interface.

Device Logging

Configures device logging parameters.

Device Log Export

Configures device logging export options.

Other Configuration

SNMP Parameters

Configures Simple Network Management Protocol (SNMP).

Preferences

Configures EIFE interface preferences.

Advanced Services Control

Configures the advanced service control parameters.

User Account

Creates and edits groups and users. Configures email accounts.

Webpage Access

Configures webpage access rights for each user group.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.