DOCA0106EN-16

Device Control

Reset Commands

The Device Control page allows you to execute one or more reset commands.

From the Control menu, in the Device Control submenu, on the device list, select the device and click Reset. Select an Operation in the Resets list to reset.

This feature is always enabled.

Application Control

The Device Control page allows you to control the following applications remotely:

  • Breaker application

  • IO application

Password Management

When the application control operation is performed, an Authorization Required dialog box appears in the EIFE webpage. Enter the password in the Authorization Required dialog box to perform the application control operation.

The password is required for MasterPacT MTZ circuit breaker with MicroLogic control units.

The following operations in the Device Control page require a password:

Control

Operation

Availability

Breaker

Open/Close

MasterPacT MTZ circuit breaker with MicroLogic control units

Light

On/Off

IO 1 or IO 2

Load

On/Off

IO 1 or IO 2

Reset input counters

I1 I2 I3 I4 I5 I6

IO 1

#I1 #I2 #I3 #I4 #I5 #I6

IO 2

Reset output counters

O1 O2 O3

IO 1

#O1 #O2 #O3

IO 2

User-defined output control

On/Off

IO 1 or IO 2

Breaker Application

From the Device Control page, in the Breaker Application, the authorized group can perform the following operations:

Control

Status

Operation

Availability

Breaker

Open/Close/Tripped/NA

Open/Close

MasterPacT MTZ circuit breaker with MicroLogic control units

NOTE: Pop-up message confirms that the command is successfully sent. It does not confirm whether the complete operation is successful.

IO Application

From the Device Control page, in the IO Application, the authorized group can perform the following operations:

Control

Status

Operation

Availability

Reset input counters

I1 I2 I3 I4 I5 I6

IO 1

#I1 #I2 #I3 #I4 #I5 #I6

IO 2

Reset output counters

O1, O2, O3

IO 1

#O1 #O2 #O3

IO 2

Light control

ON or OFF

ON / OFF

IO 1 or IO 2

Load control

ON or OFF

ON / OFF

IO 1 or IO 2

User-defined output control

ON or OFF

ON / OFF

IO 1 or IO 2

NOTE:
  • The IO application control is possible only when the IO module is connected to a circuit breaker.

  • The light and the load control are available when the application rotary switch of IO 1 or IO 2 is in position 4.

  • The user-defined output control is available only when the user-defined output has been assigned with EcoStruxure Power Commission software.

  • If the input is assigned as a pulse counter, the operation is P1, P2, P3, P4, P5, and P6 for IO 1. For IO 2, the pulse counter operation is #P1, #P2, #P3, #P4, #P5, and #P6.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.