DOCA0106EN-16

Real Time Data

Description

The Real Time Data page provides:

  • The basic readings of the circuit breaker connected to the EIFE interface in real time on Single Device Pages.

  • The circuit breaker summaries on Summary Device Pages.

  • The real-time trending for the circuit breaker for the selected topics on Trending.

NOTE: Refresh the webpage by action on the function key F5 when out of service is displayed.

Single Device Pages

This page displays the basic readings of the circuit breaker connected to the EIFE interface on real-time basis. This includes circuit breaker health status with green, orange, and red indication, cradle status, load current, power, power factor, voltage, and so on.

The table shows the steps to monitor the real-time data of a device:

Step

Action

Result

1

From the EIFE webpage menu bar, click Monitoring.

Displays the Monitoring menu.

2

From the Monitoring menu, in the Real Time Data submenu, select the circuit breaker from Single Device Pages.

Displays the real-time data of the circuit breaker.

Summary Device Pages

The summary device table views provide summary of the MasterPacT MTZ drawout circuit breaker connected to the EIFE interface.

Step

Action

Result

1

From the Monitoring menu, in the Real Time Data submenu, click Summary Device Pages.

Expands the tree for summary page selection choices.

2

Select the Summary Page to be viewed.

Displays the device selection list.

3

Select the circuit breaker from the Available Devices, then click Apply.

NOTE: Click select all to select all the available devices. Click clear all to clear all the selected devices.

Summary of the circuit breaker appears.

NOTE: Click New selection to navigate back to the device selection list.

Trending

Step

Action

Result

1

From the EIFE webpage menu bar, click Monitoring.

Displays the Monitoring menu.

2

From the Monitoring menu, in the Real Time Data submenu, select Trending.

Expands the data tree for real-time data option selection and the time trending option selection.

3

Select Real Time Trending.

Displays the real-time trending setup page.

4

Select the circuit breaker from the Available Devices list.

Selects the circuit breaker for trending.

5

Select up to 8 topics from the Available Topics list.

Selects topics for trending.

6

Click Apply to open the Real Time Trending display page.

Displays the real-time trending display page.

7

Set the trending parameters.

Allows trending parameters to be set.

Trending Parameters

Step

Action

Result

1

Select Absolute or Relative trending.

NOTE: Absolute redraws the x-axis in the graph after each sample, filling it with all the data collected since the start of the trend. The Relative updates the graph with the latest data after each sample while the x-axis stays constant to show the overall trend time selected.

Selects graph mode.

2

Choose a trend time from 1–15 minutes. This is the duration of the trend.

Selects the amount of time of the trend.

3

Select Start Sampling to start the trending of the selected topics.

NOTE: Trending may be stopped before reaching the trend time by clicking Stop Sampling. If Start Sampling is pressed after stopping the sampling, a new trend is started.

Starts trending.

4

Press Data Points to view a log of all the sampled topics recorded during the trend time.

Displays a log of all topic values sampled during the trend.

5

Press New Selection to reselect the devices and topics to trend.

Navigates back to the real-time trending setup page.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.