DOCA0106EN-13

ULP

Description

The ULP page displays the global statistics of ULP port connection.

The users with Installer or Engineer roles can consult the Diagnostics pages.

Navigation to the ULP Page

To view the ULP page, click DIAGNOSTICS > COMMUNICATION > ULP .

ULP Global Statistics

Statistic

Description

Frames Received

Number of CAN frames received successfully

Frames Transmitted

Number of CAN frames transmitted successfully

Max Receive Error

Maximum number of CAN received errors (REC)

Max Transmit Error

Maximum number of CAN transmitted errors (TEC)

Bus off

CAN Bus off count

Max Bus off

Maximum number of bus off counts

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?