DOCA0106EN-15

Redundancy-RSTP Bridge

Description

The REDUNDANCY-RSTP BRIDGE page displays the diagnostic data of RSTP bridge.

The users with installer or engineer roles can change the Diagnostics page settings.

Navigation to the Redundancy-RSTP Bridge Page

To view the REDUNDANCY-RSTP BRIDGE page, click DIAGNOSTICS > COMMUNICATION > REDUNDANCY-RSTP BRIDGE.

General Parameters

Parameter

Description

Bridge Status

Status of RSTP feature. It is either enabled or disabled based on the configuration.

Bridge ID

Unique identifier of this Bridge. It is a combination of MAC address and Bridge Priority of this device.

Root ID

Unique identifier of the Root Bridge. Combination of MAC address and Root Bridge Priority of the Root device

Root Port

The port number that offers the lowest cost path from this bridge to the root bridge.

NOTE: For the Root Bridge, the value is always 0. For other devices, either 1 or 2.

Root Path Cost

The cost of the path to the root as seen from this bridge.

Total Topology Changes

Total number of topology changes detected by this bridge since the last reset counters.

Click Reset Counters to reset the statistics values to 0.

If the EIFE interface is switched off or if it is reset due to a configuration change or another event, the statistics values are reset to 0.

Configured/Learned Parameters

Parameter

Description

Configured Bridge Hello Time

The value of Hello Time configured at this Bridge.

Learned Bridge Hello Time

The actual Hello Time used by the bridge currently. This is the configured Hello Time of the Root Bridge.

Configured Bridge Forward Delay

The value of Forward Delay configured at this Bridge.

Learned Bridge Forward Delay

The actual Forward Delay used by the bridge currently. This is the configured Forward Delay of the Root Bridge.

Configured Bridge Max Age Time

The value of Max Age Time configured at this Bridge.

Learned Bridge Max Age Time

The actual Max Age Time used by the bridge currently. This is the configured Max Age Time of the Root Bridge.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?