SNMP
Description
The page displays the diagnostic data of SNMPV1 Agent parameters.
The users with installer or engineer roles can change the Diagnostics page settings.
Navigation to the SNMP Page
To view the page, click .
SNMPV1 Agent Parameters
|
Parameter |
Description |
|---|---|
|
|
Displays the state of SNMPV1 agent. |
|
|
Number of packets received from the network. |
|
|
Number of packets transmitted from the network. |
|
|
Number of traps transmitted on detection of a change as asynchronous notification from agent to manager. |
|
|
Number of received bad community names. |
|
|
Number of transmitted bad community names. |
|
Click to reset the statistics values to 0. If the EIFE interface is switched off or if it is reset due to a configuration change or another event, the statistics values are reset to 0. |
|