Modbus TCP/IP Filtering
Description
The Modbus TCP/IP clients connected to EIFE interface.
page allows you to set the level of access forThe users with Security administrator role can edit the Modbus TCP/IP filtering parameters.
Navigation to the Modbus TCP/IP Filtering Page
To view the
page, click .Modbus TCP/IP Filtering Parameters
Parameters |
Description |
---|---|
|
Enables the Modbus TCP/IP address filtering (disabled by default). The list of IP addresses available in the table is granted access. |
IP Filtering Global Access List Parameters
Click the icon to edit the and set the access level.
Setting |
Description |
---|---|
|
Filters the required IP address you entered. A maximum of 10 IP addresses are allowed. |
|
Displays the access level for the corresponding IP address:
|
IP Filtering Exception List Parameters
Click
button and set additional parameters.
Setting |
Description |
---|---|
|
Filters the required IP address you entered. A maximum of 10 IP addresses are allowed. |
|
Displays the access level for the corresponding IP address:
|