User Management
Description
The
page is only accessible to the user with Security Administrator (SECADM) role.The users with Security Administrator role can:
-
Create, edit, and delete user accounts.
-
Assign a role and a password to the users.
Navigation to the User Management Page
To view the
page, click .Security Administrator Role
The Security Administrator user account is created by default with all the roles. Therefore, EIFE interface helps to ensure that at least one user with SECADM role is always present in the users list.
![]() |
---|
POTENTIAL COMPROMISE OF SYSTEM AVAILABILITY, INTEGRITY,
AND CONFIDENTIALITY
Change default passwords at first use to help prevent
unauthorized access to device settings, controls, and information.
Failure to follow these instructions can result in death, serious injury, or equipment
damage.
|
The Security Administrator default password is AAAAAAAA.
User Account Parameters
Parameter |
Description |
---|---|
|
Enter a name for a new user.
|
|
Enter the password for the new user Password Syntax. The password entered must be confirmed. |
|
Select one or multiple roles for the new user in the predefined list of roles Role Based Access Control. |
|
Enter a valid email address for the entered user name. |
User Account Edition
Once the user account is created, click the icon to edit and complete it with the following
parameters.
Parameter |
Description |
---|---|
|
Edit the user name. |
|
Change the role. |
|
Edit the email address of the user. |
|
Enter the phone number of the user. |
|
Select the user language in the predefined list of languages. |
|
Unlock the user account locked after entry of 3 incorrect passwords. |
|
Turn on to enable the user account. |
User Account Details
Once the user account is created, click the icon to view the following parameters.
Parameter |
Description |
---|---|
|
Displays name of the user. |
|
Displays the email address of the user. |
|
Displays the selected language of the user. |
|
Displays the phone number of the user. |
|
Displays the user status. |
|
Displays the expiration time of user password. |
l |
Displays the user account locked status. |
Password Syntax
A password is composed of 8 to 16 characters. It is case-sensitive and the allowed characters are:
-
Digits from 0 to 9
-
Letters from a to z
-
Letters from A to Z
-
Special characters as *, /, \, etc.
To be accepted by EIFE interface, a password must contain one letter lowercase, one letter uppercase, one digit and one non-alphanumeric character.
Password Customization
Once created by the user with Security Administrator role, the credentials are shared by Security Administrator with the new user.
![]() |
---|
POTENTIAL COMPROMISE OF SYSTEM AVAILABILITY, INTEGRITY,
AND CONFIDENTIALITY
Change default passwords at first use to help prevent
unauthorized access to device settings, controls, and information.
Failure to follow these instructions can result in death, serious injury, or equipment
damage.
|
The new user will be prompted to change his password at first connection. The password can be changed anytime by the user in the
window.Password Reset
A user with Security Administrator role can reset another user password by pressing the
button in the webpage. The new password is generated automatically and is shown in a pop-up message. Once generated, the new password is shared by Security Administrator with the user. The user must customize his new password at the first connection.For more information about resetting the Security Administrator password, refer to Reset Button.
In the case that all passwords with Security Administrator roles are lost or forgotten, contact your local Schneider Electric Customer Care Center.