0000649743_02_en

Attach the Lifting Eye Bolts

  1. Only for systems without rain roof: Remove the cabinet roof screws and washers.
  2. Attach the lifting eye bolts (E). Use the washers (D) from the distant bolts or cabinet roof screws.
    NOTE: The lifting eye bolts are typically delivered in a plastic bag placed under the rain roof on top of the system or inside the cabinet.
  3. Tighten the lifting eye bolts (E) to a torque of 10 Nm (88.5 lbf-in).
  4. Make sure that lifting eye bolts (E) are attached to all lifting locations.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?