0000649743_02_en

Remove the Pallet

To transport the cabinet without the pallet or to lift the system of the pallet, the pallet screws need to be removed. The cabinet is secured to the pallet with 4 screws, one at each corner of the plinth (A). To remove the pallet from the system:

IMPORTANT: Only systems where either the width or the depth is at least 800 mm (31.5 in) can be moved without a pallet. Systems with a width and depth of 600 mm can only be lifted of the pallet.
  1. Unscrew and remove the screws at each plinth corner (A).

  2. Make sure nothing else attaches the system to the pallet.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?