0000649743_02_en

Remove Lifting Eye Bolts

  1. Unscrew and remove the lifting eye bolts (E) and washers.
    NOTE: The same washers (D) are used for the distance bolts or cabinet roof screws.
  2. Only for systems without rain roof: Attach and tighten the cabinet roof screws and washers.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?