0000649743_02_en

System Space Requirements

The system has minimum clearances requirements from the top (A) and from the back (B), for airflow and to be able to transport the system. The minimum clearances depends on where the air outlet is located.

It is possible to place systems side by side. It is recommended to not have any direct contact between the side walls.

IMPORTANT: Always make sure that there is enough space for the warm air to dissipate.
Position Minimum Clearances
Top Air Outlet Back Air Outlet
(A)* 300 mm (12 in) 300 mm (12 in)
(B) 20 mm (0.8 in)* 100 mm (4 in)
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?