0000649743_02_en

Environment and Ventilation

NOTICE
System OVERHEATING
Always be aware of the space requirements around the system for ventilation and operation.
Never cover the product’s ventilation openings when the system is in operation.
Failure to follow these instructions can result in equipment damage.

For sufficient ventilation make sure that the system placement follows the minimum clearances. Make sure that the system environment is within the specifications. For information about the environment specifications, see the Technical Data.

The necessary quantity of air cooling per hour from the cooling system depends on:

  • The size and number of systems

  • The specified ambient temperature

  • The temperature of the incoming cold air from the cooling system

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?