0000649743_02_en

EPO Connection

The EPO has an internal 24 V DC power supply. It is wired to two terminals on the controller (NO), if the circuit is closed the EPO signal is sent to the controller and the modules turn off. For more information see the Drawings.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?