0000649743_02_en

Rating Plate

  • (A) System type
  • (B) System type designation
  • (C) Mains input values
  • (D) (Not used)
  • (E) Battery values
  • (F) Output values
  • (G) Protection degree and ambient temperature range
  • (H) Place for certification/conformity mark (e.g. CE, EAC, UL)
  • (I) Unique identifier and manufacturing information:
  • Gutor project number

  • System serial number

  • Transport unit number

  • Year of manufacturing

  • Country of origin / Country of manufacturing

System Type Designation

The top section (B) of the rating plate contains the system type designation. The system type designation contains information about the system configuration.

Position Description Options
(J) Gutor Modular Always GUM for all Gutor Modular systems
(K) System type
  • ADC – Rectifier system, AC to DC
(L) Maximum output power [kW] Based on customer specification
(M) Input phases
  • 1 – Single phase input
  • 3 – Three phase input
(N) Nominal output voltage [V]
  • 24, 48, 60, 110/125, 220 V DC
(O) Maximum output current [A] Based on customer specification
(P) Number of system inputs
  • None – One input
  • 2 – Two inputs, also called dual input
(Q) Module configuration
  • None – No redundancy, also called N + 0
  • N + 1 – One redundant module
  • N + x – Customized number of redundant modules, selected number will be shown. For example, N + 3.
  • N + N – Fully redundant

Unique Identifier

The bottom section (I) on the rating plate contains the unique identifier. The unique identifier is built up of sections to make it possible to identify the cabinet.

Position Name Description
(R) Gutor project number A unique number for each project.
(S) System serial number Indicates a specific system number in the project.
(T) Transport unit number The number indicates a transport unit. A system may consist of multiple transport units that can be separated for transportation.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?