0000649743_02_en

Fasten the Cabinet to the Floor

WARNING
Tip OVER HAZARD
Always fasten the system to the floor. The system has a high center of gravity.
Failure to follow these instructions can result in death, serious injury, or equipment damage.

Each system has a plinth at the bottom of the cabinet with the height of 100 mm. The plinth needs to be fastened to the floor at the installation site. At each corner of the plinth there are two different locations where it can be fastened.

For dimensions and details of the plinth, see the Drawings.

  • The location (A) is accessed from outside the cabinet by removing a cover on the plinth.

  • The location (B) is accessed from inside the cabinet by removing the bottom gland plates (C).

IMPORTANT: Always fasten the cabinet to the floor before connecting any cables.
NOTE: It is only necessary to fasten one of the locations at each corner.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?