0000649743_02_en

Transport the Cabinet with a Forklift or Pallet Truck

WARNING
Tip over HAZARD
  • Only use forklifts and pallet trucks rated for the weight of the cabinet.
  • Always make sure that the center of gravity is as close to the middle of the forks as possible.
  • Always make sure that the forks protrude on the other side of the system and that the frame fully rests on the forks.
  • Fasten the cabinet to the forklift or pallet truck.
Failure to follow these instructions can result in death, serious injury, or equipment damage.

The transportation options depend on the width and depth of the cabinet:

  • For cabinets where both the width and depth are 600 mm (23.6 in) or less, the system must be moved while on the pallet.

  • For cabinets where either the width or the depth is at least 800 mm (31.5 in) or more, the system can be moved either with or without the pallet.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?