0000649743_02_en

Lift the Cabinet with Lifting Eye Bolts

Before lifting the system, the pallet needs to be removed and if the system has a rain roof this also needs to be removed. Then the lifting eyes can be attached.

NOTE: The lifting eye bolts are typically delivered in a plastic bag placed under the rain roof on top of the system or inside the cabinet.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?