0000649743_02_en

Push In Terminals

To connect a cable to a push in terminal no tool is required.

NOTE: Only use flat screwdrivers if a cable needs to be removed from a push in terminal. Apply pressure carefully to release the cable.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?