0000649743_02_en

Transport the Cabinet without the Pallet or Lift the System Off the Pallet

WARNING
Tip over HAZARD
When transporting a cabinet without a pallet:
  • Only move cabinets with a width or depth equal to or larger than 800 mm (31.5 in) with a pallet truck or forklift.
  • Forklifts can only be used to lift a cabinet straight up if both the depth and width are less than 800 mm (31.5 in), so that the pallet can be removed from under it.
Failure to follow these instructions can result in death, serious injury, or equipment damage.

The system can now be lifted of the pallet or moved to the final installation place if either the width or depth is equal to or larger than 800 mm (31.5 in).

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?