0000649743_02_en

System Installation Location

WARNING
HAZARD OF FIRE
The system must be installed directly on a leveled, solid and non-combustible surface that can support the weight of the system.
Failure to follow these instructions can result in death, serious injury, or equipment damage.

Before starting the installation read the complete chapter and consider the systems location, space and environment requirements.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?