Lift the System and Lifting Options
WARNING |
|---|
|
Risk of Heavy Objects falling
Failure to follow these instructions can result in death, serious injury, or equipment
damage.
|
After the lifting eye bolts have been attached, lift the cabinet to the installation location.
For cabinets that weigh more than 580 kg (1279 lbs) and less
than 750 kg (1653 lbs):
Always use a lifting traverse
that strains the lifting eye bolts perpendicular (90°) to the
top of the system.
For cabinets that weigh 580 kg (1279 lbs) or less:
It is recommended to strain the lifting eye bolts perpendicular
(90°) to the top of the system. The lifting eye bolts can also
be strained at an angle. The minimum allowed angle depends on the
system weight, see table.
| System weight: | ≤ 750 kg (1653 lbs) |
≤ 580 kg (1279 lbs) |
≤ 415 kg (914 lbs) |
≤ 240 kg (529 lbs) |
| (A) Minimum strain angle: | 90° | 67.5° | 60° | 45° |
WARNING