0000649743_02_en

Transport the Cabinet on the Pallet

The cabinet can be moved to the final installation location while on the pallet.

NOTE: All systems can be moved while on a pallet. Systems with both width and depth less than 600 mm (23.6 in) can only be moved while on the pallet.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?