0000649743_02_en

Transport the Cabinet

WARNING
UNINTENDED Transportation OF HEAVY OBJECT
Never transport the cabinet with any modules or batteries installed.
Always follow the instructions for the selected recommended transport option.
Failure to follow these instructions can result in death, serious injury, or equipment damage.

There are two recommended ways to transport the cabinet to the final installation site:

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?