0000649743_02_en

IP Protection

The IP protection with the cabinet door open is always IP 20.

With the cabinet door closed, the options for the system IP rating are:

  • IP 20 (default). Includes grid in the cabinet top and ventilation grids without air filters in the door.

  • IP 42. Includes rain roof, grid in the cabinet top and ventilation grids without air filters in the door.

NOTE: Other system IP ratings might be available depending on customer needs.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?