0000649743_02_en

Attach Plinth Corner Covers

If any plinth panels were removed during transportation of the system, make sure they are attached again before attaching the plinth corner covers.
NOTE: The corner covers are typically delivered in a plastic bag placed under the rain roof on top of the system or inside the cabinet.
  1. Attach the covers (D) on each plinth corner. Carefully slide and push it into place.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?