0000649743_02_en

External Battery Breaker

If an external battery breaker is used the signal from it must be wired to the terminal in the terminal section. The terminal is connected to the controller.

For details about how to wire the external battery breaker signal see the Drawings.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?