Install Batteries
DANGER |
|---|
|
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
When working on batteries always use:
Failure to follow these instructions will result in death or serious injury.
|
The battery bank can either be internal or external. An internal battery bank is only possible in certain system designs. Due to cabinet and system design limitations, only certain batteries can be used for the internal battery bank.
For larger or higher rated systems an external battery rack or cabinet must be used.
During the battery installation:
-
Start placing the cells from the bottom, to avoid a high center of gravity in the cabinet or the rack.
-
Interconnect all the batteries with the provided cables and copper bars according to the Drawings.
IMPORTANT: Pay attention to the polarity! -
Make sure that any external battery breaker is correctly sized.
-
Check the polarity on the cable and breaker terminal before connecting.
DANGER